Other Parts Discussed in Thread: TPS40211
Hello,
I want to use the TPS40211 boost converter as a LED driver for driving high brightness LEDs from 12V input. I am looking at the application circuit in the data sheet (page 34) and have a few questions.
1. If I undestand correctly, dimming is done by pulling down the COMP pin to ground. Since the COMP pin is essentially the output of the EA, this turns off the switching, right? What is the purpose of the diode in series with the PWM FET? It doesn't seem like it's supposed to do any rectification so I suppose it's the voltage drop that is significant here?
2. I understand that R6 is the current sense resistor for the LED string and should be set so that the voltage drop across it equals Vsense when the desired current is flowing through it. But what is the purpose of R13 in this case? Is it required? What value should it be?