This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340EVM-017: Followed schematic for PCB . output is 30V instead of 24V

Part Number: TPS55340EVM-017

Hi. I have realized a standalone power supply following TPS55340EVM-017, 5-V to 12-V Input, 24-V Output Boost Evaluation Module.

After PCB arrived the output is fixed to 30V, not 24.

Have checked all components, also formula that calculates resistance value of feedback obtaining a value of 185k rounded to 187k value.

The problem is I have 30V output value.

with all load conditions,

any help? What should I consider next?

Best regards and thanks

Stefano