Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50
Hi all,
We got a customer requirement that Li-ion battery should be charging at user defined current rate than power source capability. Ex: Power source capacity is 16.4 V/ 5A. manager. The battery charging should be limited to 16.4V/1.5A only. But, it is not limiting with Set current rating instead of it is going with power source capacity. if PSU is 2 A, it is charging at 2A, if it is 3A, it is charging at 3A and so on... it is get terminated if it goes beyond Over Charge Current setting. Would it be possible to limit charging current X A based on requirement. Ex. need to limit with 1.5A.?
BQ40Z50-R2 part is used as battery pack device.
Thanks in advance for your valuable suggestion.
Regards,
Udaya