Other Parts Discussed in Thread: LP5861, LP5018
Hello there,
I've been going over the datasheet for this LED driver and am interested in using the sub address feature to control multiple RGB LEDs simultaneously. The goal would be to use a sub address to control the brightness of every LED of the same color. With the 3 sub addresses available it should be possible to control each individual color with their own unique I2C address.
The issue is that there is no mention of what output pins are associated with what sub address register. It is also unclear whether or not these associations can be controlled via the chip's registers, although there doesn't seem to be any register listed that would possibly support that feature. Any clarification on these points would be very much appreciated. Thank you for your time.