This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS272C45: Pspice file simulation profile library difficulties

Part Number: TPS272C45


Having difficulty getting the simulation profile to run without errors for the TPS272C45D testbench circuit downloaded from the TI Website.  Using Pspice for TI 17.4-2022, with the libraries path and files included (Properly?) in the simulation settings.  What should I be doing to run the extracted testbench from slvmdp8.zip ?

  • Hi Rick,

    Can you please include this attached library in addition to the library included with the zip file and retry the simulation?3250.nom.lib 

    Thanks,

    Shreyas

  • Hi, Shreyas,

    I included the 3250.nom.lib file in the simulation profile, but still have error messages.  I see the 3250.nom.lib points to a bunch of built-in library files, so I guess my Pspice installation may be somehow corrupted.  The project got de-prioritized, so I will try checking my installation when I get back to it.  TNX for the help.

  • Hi Rick,

    Thanks for letting us know. If you continue to have difficulties, another option is to acquire the EVM. You may be able to sample this with the help of your assigned TI sales representative.  You can also find these in the TI store.

    For fastest support feel free to also create a new post on E2E when you have more information to share.

    Thank you for your interest in our industrial high side switches.

    Shreyas