This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92682-Q1: Example C code / script for specific configuration

Part Number: TPS92682-Q1


team,

I was hoping the SW available on ti.com EVM-069 would contain it but it doesnt : can you please point me to the C code ( or CCS project ) containing the SPI driver and exmple code to generate working SPI frame for the 682 ?

Also can you please provide a script to configure the TPS92682 for 53V output 13ms softstart and output enable?

thanks