Other Parts Discussed in Thread: 4460
We set the current (User Rate-mA) to 1230mA (load mode=0 load select=6) and also set a constant current of 246mA for the discharge test.
However, the result looks like 1230mA is not contributing to the RM calculation.
Please help to confirm
1. my understanding is that after setting a fixed current (1230mA), the meter will calculate the RM in the discharge mode with a fixed current of 1230mA and the duration of discharge. is this understanding correct? If not correct, what should it be?
2. If #1 is correct, referring to the attached test log, please assist in identifying what is causing the test results to be inconsistent with expectations?