This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: NiMh cell charging

Part Number: BQ25713
Other Parts Discussed in Thread: , BQ25798, BQ24650

Hi Experts,

We need your confirmation with these two devices. BQ25713 and BQ25713B.

Could we connect a photovoltaic panel (Vtyp:3.6V Ityp:50mA 180mW - Voc:4.9V Vocmax:5.5V Isc: 64mA) directly on the input of the BQ25713?

Could we recharge up to 4 NiMh cells (series) with the same photovoltaic panel?

Thank you in advance for your support.

Best regards,

Jonathan