Other Parts Discussed in Thread: UCC21710, UCC21732
We are using 4 pin TO-274 SiC Mosfets and there doesn't appear to be a TI isolated gate driver chip that can do over current sensing. On the 3 pin transistors this is simple, but on the 4 pin transistor we believe we should connect the OC pin not to the positive side of the shunt where it connects to the source pin, but to connect to the negative side of the shunt or power ground. This is because the com pin on the gate driver is connected to the kelvin pin now, not the power ground.
There was a post a few years back that referred to the SLUUBX2B user guide for the UCC21732QDEVM-025 eval board, but that board had a bunch of extra components needed to mirror the voltage signal.
Is there a TI gate drive chip that can be used to perform over current detection on a 4 pin transistor without all of this extra circuitry, are we missing something?
Thanks
Dave