This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ14202: Instantaneous power supply change

Part Number: LMZ14202


Hi Team,

I designed a circuit for following conditions 

Input voltage = DC24V

Output voltage = DC 3.3 V

Q1: supplying input voltage

24V → 15 V (continued for 30 milliseconds) → 24 V

If an instantaneous power supply change occurs like above  how will the chip work?

Q2: Simulating the above case with LTSpice

Is this possible?

Best Regards,
Tom