Part Number: REF5010
Other Parts Discussed in Thread: REF102, REF50
Hello All,
I have a loadcell condition circuit. I have been using REF102A (DIP) and ADR435 IC's. After end of life of REF102 (DIP) I have made a new board using REF5010 and REF5050 pair. For 10V I have been using current boost circuit with a transistor. My maximum current for 10V is around 90mA. When there is no loadcell attached to circuit current consumption can be around 3-5mA. Transistor is BCP53/16.

I noticed there is an oscillation on REF5010. There is no problem with REF5050.
If I increase 390R resistor to 2K ripple decreases but when no loadcell attached circuit (low current) Output of REF5010 becomes Vin, which is 15V. With REF102 DIP I do not have any problem.