This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54540: Does TPS54540 Vout can quick discharge when remove the loading?

Part Number: TPS54540
Other Parts Discussed in Thread: TPS62903-Q1

Hi team,

My customer asked that can TPS54540 quick discharger when we remove the loading? they have one situation that will disable output loading and this moment would need to Vout discharge less than 10ms from 8.5V to 0V. like ON the MOS as below picture red circle to quick discharger.

BR,

Jimmy