Dear TI team
Please tell me about the CC pin connection between the "TPS25750D" and the type-c receptacle on the same board.
I think that the CC1/CC2 pins of the "TPS25750D" can be directly connected to the CC1/CC2 pins of the type-C receptacle without resistors,
because of the built-in cable detection function.
Is this perception correct?
Best Regards,
Taroimo