This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82084: VOUT rise time

Guru 10100 points
Part Number: TPS82084

Hello,

My customer measured the rise time of the TPS82084 in use and it is as follows.

Yellow is VOUT (3.3V) and green is IOUT (typical 0.92A). It is about 0.55 mS from 10% to 90% of VOUT.

Is the VOUT rise time appropriate? Are there any specifications that customers need to adhere to for the TPS82084?

Thank you.

JH