Other Parts Discussed in Thread: TUSB1044
Hi David and Zach
Thanks for your support about TUSB544. I have communicated with customer the application of TUSB544, and there are also some question.
application: used on smart phone USB port to increase signal. The USB port will automatic recognition the USB mode or DP mode by display link
question:
1.if don't use our redriver, the USB port will automatic recognition the USB mode or DP mode by display link, how to do the automatic recognition while use TUSB544. Dose it work through HPDIN pin and CC1 CC2? Is the HPDIN used to switch DP an USB? How the HPDIN pin work, can it connect with a normal GPIO of TYPE C PD CONTROLLER?
2. I find the CTLSEL Register can configure the USB mode and DP mode enable. if the value is 0x10, is it meaning only can be use at DP mode? How to configure this Register while at the scenario of the USB and DP switch by display link?