This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF5050: Spice model don´t work when in negative shunt configuration.

Part Number: REF5050

Dear technical support,

I simulated a similar circuit to the one described in the voltage reference design document of TI for negative voltage connected in shunt configuration. But, TINA TI doesn't show the values ​​correctly in the output. Instead of 5V, I´m getting 1.77V on the output when I run a DC analysis -> Calculate nodal voltage.
I think that spice model was not developed for this type of configuration.
Could someone review spice model to model shunt configuration ?

Best Regards,
Leonardo Cunha

slim174a.tsc