Hi,
I am using the TPS4H160BQPWPRQ1. If One channel output is shorted to VBAT (VBAT > VIn) and If all the channels are enabled, whether short to VBAT of one channel will affect the other enabled channels ?
I'm having 2 options for that :
1) In my design I have provided the clamped diode in Current Sense PIN which can clamp any voltage above than 1.8 V. So, If the above condition is true then shall I use the design with clamped diode to avoid the short to VBAT failure on all channels ?
2) Or if I use 4 Schottky diode on each output channels will protect the short to VBAT failure on all channels.
I want to know, which option will be better option for me, or Please suggest me if you have any option for this condition.
I have attached the schematic for reference.
Thanks