Hello,
I have two power supply challenges ahead of me that i need some help with.
1). Vin=6-18V, Vout=5V @ ~3A.
2). Vin=6-18V, Vout=+/-6V @ ~+/-20mA
The first supply is for power multiple subsystems with the use of regulators(1.8V, 3.3V...). It should be relatively clean but can always be filtered after the linear regulators.
The second supply is for an ADC analog front end and should be as clean as possible.
Any suggestions or help?
thanks
kyle