This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We have used TPS56C230RJER in our design to generate 3.3V power rail with following specs:
- Vin : 6 V - 8.4 V ( 2 cell lithium ion battery)
- Vout: 3.3V
- Iout: 8A
We used TI WebBench to design the power supply. The design report is also attached.
We have a couple of TPS56C230RJER blown up on our boards all of sudden.
We would appreciate any help to resolve this issue.
Regards,
Ajay
Hi Ajay,
Could you please share your schematic and layout for us to review?
Does the circuit perform well with 3.3V output or directly damage after power up?
Hi Athos,
Thanks for your reply.
The snapshot of the schematics and layout is attached for your reference.
The 3V3 power supply works and then randomly blows up the IC.
Regards,
Ajay
Hi Ajay,
The schematic looks good. Please add some more information.
Please also test the resistance Vin to SW and SW to GND to see if the MOS are damaged.
Hi Athos,
The answers to your questions is as follows:
The typical draw from the power supply is 1.5 A and transient load may be up to 5A.
It is a prototype stage.
This is a new design.
We have this issue on 3 of the 5 boards.
Regards,
Ajay
Hi Ajay,
we may need more information for further analysis, which needs your help.
1. Could you help summarize the other two IC's damage phenomenon and attach the burned out pictures.
2. Duplicate the damaged phenomenon and capture the waveforms(VIN, Vout, SW, Iout)
3. Test the resistance Vin to SW and SW to GND to see if the H-side MOS or L-side MOS are damaged.
4. You can also ship a board to me to test.
Any questions, pls let me know.
xueliang