Dear Team,
I'm using TPS7A2401DBVR currently.
This device is going to trigger two relays together in worst case in our design.
- The max. load is 215mA at 33ms pulse length in worst case. Then the waiting time for next pulse is very long, it's designed 5.5s min.
- We have the concern about the max. junction temp. and whether the LDO output could be switched off.
Is it possible to calculate the dynamic max. junction temp.? But we don't have its dynamic thermal resistance @33ms, and its RDS_ON (Drain-Source On-State Resistance for the MOSFET inside).
So, it would be very appreciate to give us a hint how to do this kind of calculation or support some more data?
Thanks a lot in advance!