hi.
I am testing the discharge using an electronic load.
If the current of the electronic load is increased by 1A, it operates normally up to 100A.
However, if the current is increased by 10A, if it goes up from 0A to 10A, it operates normally, but if it goes up from 10A to 20A, the gate drive is blocked and the BQ CHIP does not operate.
If the current of the electronic load is set to 0A again, it operates again.
Why is the motion stopping?