Other Parts Discussed in Thread: BQ27Z561, BQSTUDIO, EV2400
Hello,
I am working on completing a learning cycle on a BQ27Z561-R2 fuel gauge with a 385mAh single cell battery (Chem ID 0x5800). It looks to me like the learning cycle has failed because RDIS flag was set and the resistance tables are not updated during the discharge cycle. At the end of the learning cycle procedure the update status is stuck at 5 and is not updating to 6.
In which cases, negative resistance is measured?
Also can you elaborate the meaning of this "The Ra update is disabled if the charge accumulation error > 5% of Design Capacity mAh."
I am sharing the logs below.
Discharge -Relax
Charge -Relax-Discharge
In the middle of 2nd discharge cycle RDIS bit set and Ra table was not updated.
Also sharing the battery datasheet and parameters set at the start of learning cycle.
1108.GRP333736-3.8V-385mAh.pdf
| 1 | GG | Design Capacity mAH | 385 |
| 2 | GG | Design Capacity cWH | 146 |
| 3 | GG | Design voltage | 3800 mV |
| 4 | GG | Discharge current threshold | 35 mA |
| 5 | GG | Charge current threshold | 80 mA |
| 6 | GG | Quit current | 25 mA |
| 7 | GG | Term Voltage - IT Config | 3000 mV |
| 8 | GG | FC Set Voltage threshold | 4400 mV |
| 9 | GG | FC Clear Voltage threshold | 4100 mV |
| 10 | GG | FD Set Voltage threshold | 3000 mV |
| 11 | GG | FD Clear Voltage threshold | 3300 mV |
| 12 | GG | TC Set Voltage threshold | 4400 mV |
| 13 | GG | TC Clear Voltage threshold | 4100 mV |
| 14 | GG | TD Set Voltage threshold | 3000 mV |
| 15 | GG | TD Clear Voltage threshold | 3300 mV |
| 16 | GG | Load Select | 1 |
| 17 | GG | Load Mode | 0 |
| 18 | GG | Cell1 Chg Voltage at EoC | 4400 mV |
| 19 | ACA | Charge term taper current | 37 mA |
| 20 | ACA | Charge term voltage offset | 100 mV |
| 21 | ACA | Charge Term Charging Voltage | 4400 mV |
Thank you,
Jainam Shah