Hi Expert
my customer application scenario as below:
Input voltage: 5V output voltage: 0.85V Iout max: 3.5A f=1.8M RF=100K
L=220nH input cap: 30uF+100nF output cap:4*22uF mode pin tie to Vin(FPWM mode) Css=47nF
Power up when full load, the SW will unstable as below: Vin=4V Iout=3.5A


increase input voltage: Vin= 5.5V Iout=3.5A


I guess it relate to comp, so I change the 100K to 10K and then doesn't have above issue but Comp 1 doesn't suitable for customer because Comp 1‘s output dynamic not good enough. so customer need choose Comp 2.
My question is:
1. why have above issue?
2. How to let device work on Comp 2 and doesn't have above issue?