This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Inverting buck recommend

Other Parts Discussed in Thread: LMR43610-Q1, LMR36503

Hi team,

I want to find a buck that support below conditions. The background is that I want to use it to output -20V. And I can't find a suitable device in TI.com. The actual input voltage is 2.5-5.5V. Considering the stable running condition, the maximum input should be over 5.5V+20V = 25.5V.  

Vin = 2.5- 25V.

Iout = 20mA.

Best Regards,

Peter