This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR50410-Q1: IC getting burned/ short issue

Part Number: LMR50410-Q1

Hi Team,

I'm testing 5VD and 3.3VD power supply which takes 24VDC as input. Reference schematic attached below. 

Circuit consumes 9mA at 24VDC under no load. 

U2 IC which converts 5VD to 3.3VD got burned near pin5 (Vin) and pin 4 (EN)  immediately after power up.

3 out of 5 samples got this issue, rest 2 of the samples are working fine.

Is there any component in the schematic which could have cause this issue.

Thanks,

Yatin