Dear engineers of TI:
1、Subclass ID:36, Offset:7
Why the default value is set to 5℃?
What is the amount of change in RM and FCC when the temperature changes by 5°C?
I think that the smaller the setting value, the better the accuracy. What is the reason for not making it smaller?
2、Subclass ID:80,Offset:20
On what basis is Res V Drop=50mV set?
3、Subclass ID:80,Offset:68&70
What is the definition of delta voltage? (Is delta voltage the change in voltage when discharged from a non-discharged state?)
What is delta voltage used as a parameter for? (Is it a calculation parameter for discharge capacity?)
What is the basis for setting Min Delta Voltage=0mV?
What is the basis for setting Max Delta Voltage=200mV?
thanks!