Other Parts Discussed in Thread: LM74900, , LM74700-Q1
Hi, Support Team
We Would use as below architecture as below chart, and some question( for ADAS application/Battery in 12V)
Q1: Would you recommend using this architecture, or do you have any recommendations?
Q2: What is the difference between LM74900/910? Which one do you recommend for implementing in Fig 1.
Q3: If the input bead, common mode choke, and PI filter are removed, can it pass the AC Superimpose Test?
Q4: Is there difference between testing VBAT1 and VBAT2 separately versus testing them together for the AC Superimpose?
Fig1.
if any suggestion. Please advise me.
Thanks,
Best regards,
Lawrence