Hello all,
I'm considering TPS2546 to manage a USB 3.0 charging port in a design based on a Jacinto 6 processor. This USB port will be used mainly in host mode, but sometimes we will need it to be in device mode.
The idea is to connect USB_DRVBUS to the TPS2546 EN pin to enable de power switch only in device mode. Unfortunately, I have detected while EN=0 not only the power switch is OFF but also the data signal switches and this is something that goes against having the USB in device mode since I need the data lines.
Since:
- The only TSP2546 modes I will use is SDP and CDP
- I suspect the data lines switch purpose is only to toggle between the different DCP divider modes
My question is: Would be OK to bypass externally the TPS2546 data lines switches by doing any of the following options, so I would have the data lines available in device mode (EN=0)?
Thank you very much in advance!