Other Parts Discussed in Thread: TPS54620
Hi,
Can we use 100uF and 220uF Ceramic caps as an Cout with TPS54320/TPS54620 Devcie.
Generating 1.1V, 1.2V and 1.5V supply voltages from 12V input. Below is the information regarding DC-DC and output voltage/current and Ceramic Caps.
| S.No | DC-DC Converter | Output voltage | Output current | Output CERAMIC Caps |
| 1 | TPS54320 | 1.5V | 1.5A | 3x 220uF , 6.3V |
| 2 | TPS54620 | 1.2V | 3A | 4x 220uF , 6.3V |
| 3 | TPS54320 | 1.1V | 2.5A | 5x 100uF, 6.3V |
Please provide your feeback on the same.