Other Parts Discussed in Thread: LP55231
Hi,
We are using two LP55231 to drive 4 RGB LEDs, each chip is driving two LEDs respectively.
Below is the configuration:
1) LP55231 is configured to use internal clock
2) Using Engine program code to drive the led patterns, ramp up/down
3) Using Trigger signal to sync two lp55231 chips, one master and other slave
When we set the pattern to blink all leds at the same time, we see at the beginning all 4 leds are in blinking at the same time as expected.
But after some time they goes out of sync.
Could you please help us understand what could be causing the issue?
We also noticed that , some time for the below engine code, even though leds mapping is fixed, leds starts functioning properly , but after some time , the leds becomes off or turn into different colors.
when we dump 0x70/0x71 register, the values are changing randomly. Could you please help us understand in what condition , led mapping changes randomly?
Example engine code
engine 1: