This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual ±200V output power solution



HI, team:

    My customer is finding dual ±200V or ±100V  without  transformer power solution, could you give some suggestions?

    Input 12V, output ±200V or ±100V, 0.1A is enough. 

    Hope to get your reply!

  • Hi Hailey,

    Any PWM controller can be used to make a boost or inverting boost converter. See the following application note (SNVA856B) on how this is done. The UCC28C50 might be a good solution to make this happen. Without a transformer-based solution, you would need two controllers. One for the boost and another for the inverting boost. 

    I hope this answers your question.