This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: Backfeed acceptable?

Part Number: TPS54331


Hi

I have a situation where I have to sources that feed a single 5V rail.

One is the output from a boost converter that feeds of a battery. The other is a TPS54331. Is there any problem with backfeeding the output? VIN will be low during those conditions