Hi David,
while I read the datasheet, I notice DP input has linear VOD setting,
since DP source output 600mV now, the signal swing voltage probably be lower when reaching our IC, so either setting should still within the linear region I supposed.
so is there a recommendation on this setting?
larger maximum tolerant swing(DP_VOD=0) is always better right?