Hi all,
I need to get +/- 5V from the usb bus (+5v) with low current. Could you tell me if TPS60400 is the best option for this application and if there´s any application note regarding this?
Thanks in advance and best regards,
Patricio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, this is the simplest way to do it. But note that you won't get a regulated -5V--it will vary based on the USB voltage and load. If this is ok, then do it.
The other optin is to use the TPS62120/2 in an inverting buck boost topology. We hope to have an app note on this in the next month.