This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5119: Review Design for LM5119 Dual Output

Part Number: LM5119

Hi!

I have recently finished a schematic for a LM5119 Dual Output design. I was hoping to have it reviewed to see if any parts of the design need to be changed. Attached is the schematic. I used the LM(2)5119 Calculator to get most of my values, just want to verify it would hit the specification target.  

Here are the following specifications I am trying to meet:

Input Voltage: 48V

Output Voltage Channel 1 / Channel 2: 40V

Output Current Channel 1 / Channel 2: 10A maximum 

Fsw: 230kHz 

K Factor: 2.8 

UVLO Voltage: 12V 

Important Parts: 

Q1, Q2, Q3, Q4: BSC027N06LS5ATMA1 (Vds 60V, Id 100A, Rds 2.3 mOhm)

L1, L2: 7443556110 (10uH, Current Rating 15A, DC Resistance 6.9 mOhm)

D1, D2: PMEG6010

LM5119 Review.pdf