Other Parts Discussed in Thread: BQ27220, BQ34210-Q1, BQ4050
Hello,
We had selected the 27220 as our fuel gauge but this device is only available in a small geometry
BGA package. This is pushing the requirements for the board (drill sizes) in order to use this device.
Can you please recommend a few additional fuel gauges that are available in larger packages?
Our product is a low-power, solar rechargeable sensing device. We are currently using a single
LI-Poly battery. The current battery capacity is 2500mAH. This is sized to provide a buffer for long overcast periods.
Thanks,
John