This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: PGOOD Pin not working

Part Number: LM5069


I'm using LM5069MM-1 for Power Supply and Inrush Control in the system.

Operating Voltage : 48V to 56V, Max. Current : 30A

PGOOD pin of the controller is pulled up to the output voltage with 100K resistor. I'm using this pin as a feedback to the microcontroller

Currently, microcontroller is not getting any feedback from PGOOD pin. Resistance between PGOOD pin and GND is 5 Ohm. although the UVLO and OVLO is functioning properly.

What could be the reason for this? Is this a know issue?