I found the other post about this but still have questions. I am not using a thermistor and the datasheet doesn't do a good job of explaining the internal circuitry.
My circuit is powered from the battery only. From the reference schematic, can I drop the 1.8M, 18.2k, and 1k resistors and tie BI/TOUT to ground? I am not sure how the thermistor measurement works (and what the 1k resistor is for). Does the gauge output 2.5V on BI/TOUT and measure the voltage at TS? In this case it seems I would want to tie BI/TOUT to ground through a resistor so it doesn't short.
Can TS be left floating? Should I tie it to ground through a 10k resistor? Or should I implement all the discrete components in the reference schematic and use a 10k to ground at the "thermistor input" node?