This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130: Device specification

Part Number: TPS65130


Hi team,

I have two question about changes from Rev.D to Rev.E. 

- Changed ESD HBM specification from "±2000" to "±1000"

What is the reason for changing to 1 kV? Was 2 kV a typo?

• Changed text string in Section 8.2.2.1.1 description From "....to set the divider current at 5 μA or greater" To
"...to set the divider current at 5 µA to 10 µA" .

If I set divider current above 10uA, will it affect operation or reliability?

Best Regards,

  • Hi Hirotsugu,

    1. - Changed ESD HBM specification from "±2000" to "±1000"

    The history behind this change is that our product line did some qualification testing back and found that the device only passes 1KV. So we changed the datasheet to reflect the correct specification.

    2. • Changed text string in Section 8.2.2.1.1 description From "....to set the divider current at 5 μA or greater" To "...to set the divider current at 5 µA to 10 µA"

    It's recommended to set the divider current in this range of 5uA to 10uA to avoid potential risk on loop stability.

    BR

    Patrick