Hi team,
I have two question about changes from Rev.D to Rev.E.
- Changed ESD HBM specification from "±2000" to "±1000"
What is the reason for changing to 1 kV? Was 2 kV a typo?
• Changed text string in Section 8.2.2.1.1 description From "....to set the divider current at 5 μA or greater" To
"...to set the divider current at 5 µA to 10 µA" .
If I set divider current above 10uA, will it affect operation or reliability?
Best Regards,