Other Parts Discussed in Thread: LMR51440,
Hi team,
I want to find a buck that support below conditions. The background is that I want to use it to output -20V. And I can't find a suitable device in TI.com. The actual input voltage is 10V. Considering the stable running condition, the maximum input should be over 10V+20V = 30V.
Vin = 10-30V.
Iout = 20mA.
I checked in TI.COM and found TPS62933P from MVB and LMR51440 from WVB. Do you have any other recommendation?
Best Regards,
Peter