Other Parts Discussed in Thread: TPS54260
Hi ,
I am using TP54160 and TPS54260 on my project. It is waken up external source via EN pin. But i catched a different condition.
If voltage is applied to the en pin while the vin is energized, I see a low negative pulse on GND.

If voltage is applied to the VIN pin while the EN is energized, I see a high negative pulse on GND.

Such a large surge damaged some of my components. The load on 5V hasn't changed when taking these measurements, and I'm not working in light load conditions. My rated output current is at least 800mA.
I'm trying to understand why feeding the EN pin before the VIN makes this difference. And can I solve the problem in a way that will provide this condition?