Other Parts Discussed in Thread: TPS65261, TPS65261-1
Hi Experts,
Our customer is going to use a Spartan 7 FPGA from Xilinx as the control device. For its power supply (1V, 1V8, and 3V3), He is considering the use of a PMIC instead of 3 converters. The PMIC will be supplied with an input voltage of VIn=12V and the estimated consumption of each output is as follows 0.7A@1V, 0.2A@1V8, 0.3A@3V3.
I hope you can help us. Thank you.
Best regards,
Gerald