This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: UCC28070PWR max BW operating - Power factor correction not required

Part Number: UCC28070

Hello,

I wanted to use UCC28070PWR mainly as boost converter with max Bandwidth possible.

I need to convert an existing PFC ckt with good PF to a "solid rock" voltage regulated o/p ( same voltage level ), in this case, it does not does not require power factor correction.

It needs to respond to load transients and avoid voltage dips caused by low BW.

Can you recommend what changes needs to be done?

Vin=180Vac-264Vac.

Vout =  380Vdc.

Po = 2kW

Thanks,

Norman