Hello,
I have been trying to drive the capacitive load on the evaluation module with the pre-charge disabled. All the protections have been disabled as well; overcurrent, short circuit, and over temperature. The EN/UVLO is connected to Vaux. When I drive INP high whilst INP_G is low, it still sets of the FLT_I flag even though all the protections are disabled. This is what I did to disable each protection on the EVM:
Overcurrent - shorted CS+ and CS- with wire and shorted IWRN to ground with zero ohm resistor.
Short circuit - shorted ISCP ad CS- with zero ohm resistor
over temperature - removed Q6
I was wondering why this is the case and if there are other mechanisms that could set of the FLT_I flag.
Best regards,
Keerthi