This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616EVM-021: Cell monitoring without passive balancing?

Genius 17475 points
Part Number: BQ79616EVM-021
Other Parts Discussed in Thread: BQ79616

Hi Experts,

Can this board BQ79616EVM-021 be operated for cell monitoring only without passive balancing?

Thank you.

Regards,
Archie A.

  • Hello,

    Cell balancing is not needed for the 616 to complete monitoring--cell balancing is a feature offered by the BQ79616, but the device must be configured to set up cell balancing before any cell balancing will be performed.  

    Also note that if the BAL_GO bit remains 0 and is not set to 1, then no cell balancing will occur.  More information on cell balancing settings and configuration can be found in section 9.3.3.1 of the BQ79616 datasheet.  If you have any trouble accessing the datasheet, please let me know.

    Best,

    Andria