Part Number: UCC27611
Other Parts Discussed in Thread: CSD17313Q2
Hi,
I am using the UCC27611 to drive a GaN Fet (EPC2204). The rise and fall times in my current design do not match what is in the datasheet.
I do get 5ns fall times, however, the rise times are around 20ns. I need <10ns rise times for my application to work correctly. I have tried reducing the gate resistors down to 0 ohm, but unfortunately 20ns rise times is still the best I am seeing.
I am powering the UCC27611 with 5V VDD. I have a suspicion this might be the issue causing the slow rise times. The datasheet seems to use VDD 12V for most of the specs listed. Does VDD have an impact on rise and fall times? Is there a graph or any extra data available for the UCC27611 detailing VDD vs rise/fall times?
I want to verify raising VDD to 12V or higher will reduce the rise time down to <10ns before I redesign the circuit.
Thanks!