We have noticed that with VBUS at 0V or completely disconnected from a source, and with all FETs turned off, we see a sizeable 50uA coming from the HS pin, to the switch node, and then to ground, through any circuit elements living on the switch node.. We know it's not leakage through the bootsrap capacitor because we can DNP it a still see the 50uA. We know the 50uA persists because we can add a 100kOhm resistor from the switch node to ground and see 2.5V develop and hold across it. We know that the FETs are not the leakage path because the gate signals are low and VBUS is low or not connected to a power supply.
This 50uA is enough to charge our output capacitor bank in a few minutes and seems high.
Is this normal operation for the gate driver?