Other Parts Discussed in Thread: LM2596, LM2595
I am using LM2596 Device.
Our application is:
Vin=5V,Vo=3.8V,Io=1.7A
- We used 33uH inductor and we observed two types of inductor current waveform at Vin, why this type of behaviour of the device.
Also above 7.3V input voltage inductor current same behaviour like in input 5.6V waveform.
We used Resistor value is Rup=2.2k ohm,Rlower=1.1k at feedback pin and Cff=10nF.
Device power up by DC power source.
Pls refer attached file i.