This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2594: LM2594 5V current rating

Part Number: LM2594


Hello, the LM2594 voltage starts to sag under load, replacing the catch diode with a schlocky, appears to correct the sag, allowing the PCBA to operate normally   

Can the output current be increased to 400mA  by replacing the 220uH with a 100uH inductor, if so what are the ramifications? 

Can you suggest a method to increase the current, The input voltage is 24V 

Replacing the 220uH inductor with 330uh had no effect.